Skip to content
LAPP Singapore logo for industrial cable and connectivity solutions provider
Spend SGD 200 more for FREE shipping.
FREE shipping will be applied at checkout

Your cart is empty

Continue shopping
0Cart(SGD 0.00)

BEYOND CABLES: LAPP DESIGNS AND MANUFACTURES EPIC® INDUSTRIAL CONNECTORS

Did you know LAPP makes industrial connectors? LAPP engineers and produces EPIC® industrial connectors for power, signal and data transmission in harsh industrial environments. The EPIC® range covers rectangular connectors and circular connectors in the M-series sizes, rated for the vibration, moisture and chemical exposure that standard commercial connectors are not built to survive. The same company that supplies your ÖLFLEX® cable also supplies the connector that terminates it.

That last point is the one most engineers miss. LAPP is known across ASEAN as a cable company, and the connector on the end of the cable often gets sourced separately, from a different vendor, on a different lead time, against a different specification. This article covers what the EPIC® range actually is, how it pairs with LAPP cable, which connector type belongs in which application, and what changes when both sides of the connection come from a single source.

What Are EPIC® Industrial Connectors and Why Do They Matter?

EPIC® is LAPP's industrial connector range. It exists because a cable is only as reliable as its termination.

In practice, the connector is where industrial connections fail. The cable itself is usually specified carefully, against flex cycles, temperature and chemical exposure. The connector is then chosen on price and availability, and it becomes the weak point: the contact fatigues under vibration, the seal fails under washdown, or the housing cracks under mechanical load.

EPIC® connectors are designed for that environment rather than for a benign control cabinet. The range covers rectangular connectors, which carry multiple power and signal circuits through a single housing and are the workhorse of machine building, and circular connectors in the M-series sizes, which handle sensor, actuator and servo connections where space is tight and the connection is made and broken regularly.

For the exact contact counts, current and voltage ratings and IP protection class of any specific EPIC® part, the product catalogue is the source of record. Ratings vary considerably across the range, and a single figure quoted for "EPIC® connectors" would be wrong for half the portfolio.

How Do EPIC® Connectors Integrate with ÖLFLEX® Cables?

This is the part that changes procurement, not just engineering.

When the cable and the connector come from two vendors, three things go wrong. Compatibility becomes your problem: cable outer diameter, conductor cross section and shielding construction all have to match the connector's clamping range and contact system, and if they do not, you find out at assembly. Responsibility becomes ambiguous: when a connection fails in service, the cable supplier points at the connector and the connector supplier points at the cable. And lead times decouple, so a machine waits on whichever half arrives last.

Specifying ÖLFLEX® cable and EPIC® connectors together removes those three problems. The cable and the connector are specified against the same duty cycle, the clamping range is confirmed against the actual cable, and there is single-source accountability if the connection fails.

That is integrated connectivity, and it is the practical reason to know that LAPP makes both.

EPIC® Connector Types for Every Industrial Application

Choosing within the range comes down to what the connection has to do.

Rectangular connectors suit machine building and panel building, where a single housing carries power, signal and sometimes data into or out of a machine section. They are the right answer when you have many circuits to route through one mechanical interface, and when the connection is made once at commissioning and rarely broken afterwards.

Circular M-series connectors suit sensors, actuators, servo motors and field devices. They are compact, they are made and broken frequently in service, and they are the standard interface in factory automation. Our M-series comparison article walks through when to choose M8, M12, M17 or M23.

Solar and specialist connectors cover renewable energy and other application-specific interfaces.

If you are new to the terminology, the industrial connectivity glossary defines the terms used across this range, and the EPIC® comparison article sets EPIC® against the alternatives you are likely evaluating.

Why Choose LAPP Connectors Over Competitors?

Because LAPP is not a reseller. LAPP designs and manufactures the connector, which means the specification, the tooling and the quality control sit inside one company.

For over six decades LAPP has built its reputation on reliability in industrial connectivity, and the EPIC® range is not a new venture bolted onto a cable business. It is a manufactured product line with its own engineering behind it.

The practical advantages are the ones that show up on site. One specification conversation instead of two. Confirmed compatibility between the cable and the connector rather than an assumption. Regional support across ASEAN through LAPP SEA, so the specification question gets answered locally rather than escalated to another timezone.

Talk to Our Engineers

If you are specifying a connector and you are not certain which EPIC® type fits the duty cycle, do not guess from a datasheet. The failure modes in industrial connections are specific to the application, and the right answer depends on vibration, ingress, mating frequency and what the cable on the other side is doing.

Talk to our connectivity specialists at lapp.com.sg/pages/contact-us, or send an enquiry through the LAPP APAC contact page. Browse the full EPIC® range in the APAC catalogue or the EPIC® product catalogue.