ETHERLINE® PROFINET: WHAT CHANGES WHEN YOU SPECIFY A PROFINET CABLE
What is the difference between PROFINET Type A, Type B, and Type C cables? Type A is a fixed-installation cable for static cable trays and conduit runs. Type B is a flexible cable rated for occasional movement, suitable for cabinet-to-machine drops or hinged panel doors. Type C is a continuous-flex cable designed for drag chains, robotic dressing packs, and other repeated-motion installations. Specifying the wrong type for the duty cycle is a recurring cause of PROFINET underperformance in service.
For controls engineers, PLC programmers, and system integrators on Siemens-led platforms, PROFINET is not generic industrial Ethernet with a green jacket. PROFINET cable carries a PI conformance specification that covers conductor diameter, shielding, jacket colour, and construction class, and the choice of cable defines what the network can do for the lifetime of the install. LAPP makes cables AND connectors for PROFINET under one engineering programme, with the ETHERLINE® PN range covering Type A fixed-install, Type B flexible, and Type C continuous-flex variants, and the ETHERLINE® ROBOT PN family certified for high-cycle drag-chain and torsion duties.
What Is the Difference Between PROFINET Type A, Type B, and Type C Cables?
Type A is for fixed cable trays, conduit, and runs that do not move after install. A Type A cable can use solid copper conductors, which improves attenuation across longer runs but does not tolerate repeated bending after install.
Type B is for occasional movement. Cabinet doors that open and close, machine guards that hinge, and drops that are moved a few times across the install life are typical Type B territory. Type B cables use stranded copper conductors and a slightly more flexible construction than Type A.
Type C is for continuous motion. Drag chains in AS/RS rigs and stacker cranes, robotic dressing packs, and AGV masts are Type C duty cycles. Type C cables (including the robotic variants such as ETHERLINE® ROBOT PN) use fine-strand copper conductors, specific lay-lengths, and abrasion-resistant jackets designed for repeated bending and torsion. The specific bend radius and published cycle count come from the cable datasheet.
The risk pattern is consistent. A Type A cable in a drag chain typically fails well inside the design life. A Type C cable in a fixed tray is over-specified for the duty cycle and wastes capital cost. The right answer comes from matching the cable type to the motion environment, not from defaulting to the highest type “to be safe”.
When Should You Specify 4-Core 100 Mbit/s vs 8-Core Gigabit PROFINET?
PROFINET supports two electrical formats. Standard 100 Mbit/s PROFINET runs on a 2-pair (4-core) cable. Gigabit PROFINET (PROFINET over Gigabit Ethernet) runs on a 4-pair (8-core) cable, the same as standard Cat.6 or Cat.6A office Ethernet but built to PROFINET conformance.
The decision sits in the network architecture, not in the cable. If the topology is locked at 100 Mbit/s across every segment and there is no migration plan, 4-core PROFINET (Cat.5e class) is the right spec. If the topology includes any gigabit-capable nodes (machine vision over the same PROFINET trunk, IRT motion control that the integrator has specified at gigabit, or a planned migration to gigabit backbone), the spec moves to 8-core (Cat.6 or Cat.6A class).
The hidden trap is that the choice is locked at cable specification. A 4-core PROFINET run cannot be retrofitted to gigabit without pulling new cable. Specifying 8-core at install for the runs that will plausibly migrate (typically the trunk and the high-bandwidth machine groups) is much cheaper than re-pulling cable two years later.
For the broader single-source story across industrial Ethernet cable and termination, the Integrated Connectivity blog covers the procurement pattern in more detail.
ETHERLINE® PROFINET Range: Cat.5e for Standard Drops, Cat.6A / Cat.7 for Higher Bandwidth, ROBOT for Drag Chain
The ETHERLINE® PN range is structured by performance class plus duty cycle. Cat.5e PROFINET (ETHERLINE® PN Cat.5e in fixed, FLEX, or FC construction) covers standard 100 Mbit/s drops. Cat.6A PROFINET adds gigabit-capable performance for vision and IRT-class motion control. Cat.7 variants (such as ETHERLINE® PN Cat.7 FRNC FLEX) push to higher bandwidth and tighter alien-crosstalk margins for the most demanding installations.
For drag chains, dressing packs, and continuous-motion runs, the ETHERLINE® ROBOT PN family is the dedicated Type C variant, with published cycle ratings for the chain-bend and torsion duty cycles. The procurement pattern is to specify Type A across fixed trays, step up to Type B at hinged cabinet doors, and reserve Type C / ROBOT for the runs that actually move continuously.
The matching connector side matters as much as the cable. EPIC® data connectors, M12 D-coded for 100 Mbit/s PROFINET and M12 X-coded for gigabit-class PROFINET, complete the channel. Specifying the connector against the cable conformance class is the most reliable way to keep the installed channel inside the PI conformance envelope.
How Do You Verify a PROFINET Network Stays Healthy in Service?
PROFINET cable health is not a one-time test at commissioning. A passing channel report on day one does not mean the channel will still meet conformance after two years of vibration, thermal cycling, and chemical exposure. The honest answer is to specify network monitoring at the spec stage, not bolt it on after an outage.
Cable monitoring tools such as ETHERLINE® GUARD monitor live PROFINET segment health and surface degradation indicators before they become a network outage, per the GUARD product page. Specifying GUARD at install gives the operations team a baseline plus a trend, rather than the binary working / broken state that traditional channel testers report. The same principle applies to the active infrastructure: an industrial-grade PROFINET switch with managed diagnostics (such as the ETHERLINE® ACCESS family) closes the loop on link health for each port rather than each segment.
The procurement signal is simple. If the line cannot afford an unplanned outage from a cable failure, the BoM should include monitoring at install rather than after the first outage drives the discussion.
Talk to Our Engineers
PROFINET cable specification is a per-segment decision (type, conformance class, core count, monitoring), not a category-pick exercise. The LAPP SEA PROFINET team can sit with your controls and integrator teams, walk the architecture, and put a spec on each segment that matches the motion environment, the bandwidth, and the lifecycle monitoring plan.Talk to our engineers about your PROFINET specification, an existing-segment audit, or any specific Type A / B / C question.