Skip to content
LAPP Singapore logo for industrial cable and connectivity solutions provider
Spend SGD 200 more for FREE shipping.
FREE shipping will be applied at checkout

Your cart is empty

Continue shopping
0 Cart (SGD 0.00)

EV Charging Cables and Assemblies: Specifying the LAPP E-Mobility Range

EV CHARGING CABLES AND ASSEMBLIES: SPECIFYING THE LAPP E-MOBILITY RANGE

What actually goes on the cable schedule for a new EV charging site? More than the cable to the gun. A charging site needs cables rated for outdoor Southeast Asian conditions and for the current each session will really draw, and it benefits from factory-assembled charging cable assemblies built and tested to length, so that termination comes off the critical path. LAPP treats e-mobility as a cable and cable-assembly segment, and the exact type for AC or DC charging should be confirmed against the LAPP catalogue before anything reaches a bill of materials.

Our earlier piece on EV charging infrastructure covered the site level, from grid connection through the charger to the gun. This one sits underneath it. Same site, different layer: the charging cables themselves, and the assemblies a charge point operator or EPC contractor actually puts on an order.

What makes an EV charging cable different from a standard industrial cable?

Duty cycle, mostly. A control cable inside a panel is installed once and then sits still for a decade. A charging cable gets pulled off its holster, dragged across concrete, coiled back up, and every so often driven over. Several times a day, every day, for years.

That changes what the specification is really about. Flexibility and abrasion resistance stop being nice-to-haves and become the properties the cable is chosen for, because the damage most sites see first is to the jacket, at the point where the cable drags.

Outdoor exposure is the second one. The cable lives in sunlight, rain and standing humidity rather than inside a cabinet, so UV stability and water resistance belong in the specification rather than in the assumptions. We went through that failure mode in more detail for solar and wind sites, and the mechanism is no different here.

Current under repeated cycles is the third. A conductor sized comfortably for an overnight AC session can run warm once the same site starts turning DC fast charges back to back. Sizing against the busiest realistic hour rather than the average one is the safer habit.

There is a split inside the range itself, too. AC charging and DC fast charging ask different things of the cable, and the DC case adds sustained conductor heating on top of everything the mechanical duty already demands. They are specified as different cable types rather than as one type in a different length.

LAPP engineers and produces both the cable and the finished assembly, which is why the e-mobility range is organised as a cable and cable-assembly segment rather than as a single product. Rather than quote a rating here that may not match the variant you order, check the type against the LAPP e-mobility pages and the published product specifications before it goes into a schedule.

Why specify factory-assembled charging cable assemblies over on-site termination?

Labour, repeatability and traceability. Hand-terminating charging cables on site puts a skilled task on the critical path at the stage of the programme with the least room for it, and it leaves a joint that was made once, by hand, in the field.

A factory-assembled charging cable assembly arrives built and tested to length. The termination was made under production conditions with the same tooling every time, and it comes with build documentation. That last part matters more than it sounds. Intermittent faults on a charging bay are among the more expensive things to chase, and being able to identify a cable and its termination from a build record narrows the search early.

Tested to length is worth reading literally. The assembly is made to a stated length and electrically tested as a finished item before it ships, so what arrives on site has already been proven as an assembly rather than as a reel of cable and a bag of parts.

Picture a highway charging hub with a dozen bays going in across a six-week window, where the electrical contractor is sharing the site with the civil works and the commissioning date will not move. Every hand termination there is a task that has to be scheduled, inspected and signed off. Assemblies that arrive tested to length turn that into an install-and-connect job, which is the difference between a trade that can absorb a delay elsewhere on the programme and one that cannot.

A charging cable assembly is also one of the clearer cases where cables and connectors have to be specified together rather than bought separately, because the assembly is the cable and its termination as one tested item. This is the work LAPP Harnessing Solutions does, and the charging assemblies sit alongside the wider cable assembly range.

One boundary is worth stating plainly. The assembled charging cable, including the vehicle-side connector on it, is in scope for this kind of specification. The charge point's own socket and its power electronics stay with the charger OEM, and the grid-to-charger site routing belongs to the companion piece rather than to this one.

How do you select charging cables for DC fast-charging sites in Southeast Asia's climate?

Environment first, then electrical duty, then build. In this region the environment is doing more work than a single temperature line on a datasheet suggests. Sustained heat, high humidity, monsoon rain and strong UV act on the same jacket at once, outdoors, continuously.

We looked at what tropical heat does to DC cabling on solar sites, and DC charging infrastructure sits in a similar place: high direct current, outdoor routing, a long service expectation.

Inside the cabinet, the DC conductor decision is its own question. Copper and aluminium behave differently on sizing, termination and cost at scale, and it is worth settling that deliberately rather than by default.

Two adjacent items usually get specified in the same conversation. ÖLFLEX® power and control cable covers the DC-side cabling inside the cabinet, and a SKINTOP® cable gland handles the enclosure entry, where the cable passes into the housing and the seal has to hold in driving rain. Confirm both against their own datasheets rather than the e-mobility pages, because their ratings are specified separately.

Mechanical protection at the pedestal deserves its own look. The cable's worst moment is usually not in free air but where it enters the charger housing, or where it is retained at the holster, because that is where the same bend happens over and over. Getting the entry, the strain relief and the bend radius right at that one point takes out a common cause of early failure.

How much of this applies varies by site. A covered urban car park in Singapore and an exposed highway fast-charging hub in Indonesia are not the same specification problem, even with the same charger on the pad.

Talk to Our Engineers

If you are putting a cable and assembly schedule together for a charging site, the useful next step is a conversation about the actual duty rather than a catalogue page. Send the site details, the charging power and the routing, and our connectivity specialists can work through the cable types and the assemblies with you.

The details that shorten that conversation are the charging power per bay, whether the site is AC, DC or mixed, the cable run and the assembly length you need, the routing and mounting arrangement at the charger, and the exposure the cable will really see. Those five turn a general enquiry into a specification.

Talk to our engineers through the LAPP enquiry form. For current catalogues and datasheets, start from the EV charging pages or the download centre.